CW10.5 debug issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.5 debug issue

2,143 Views
kevinmc
Contributor II

Hi,

I'm running a project succesfully in CW10.3, now I've updated to 10.5 and I get the following problem when trying to debug via ' download':

INF:CRC-16 Error in block. (File = $892C, Device = $2DD1)

It appears to compile and download without issue, however it falls over on checking?

We can debug using 'attach'.

What has changed here in CW10.5?? I would really like to use 'Download' debug method.

Cheers,

KMC

Labels (1)
0 Kudos
Reply
3 Replies

1,929 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Kevin:

Could you provide more details? What is the specific error you see?

If possible please share a screenshot of the issue. Also it is always good to try with a new bareboard project to determine if the problem is with CodeWarrior <-> debugger tool or specifc to your project.


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,929 Views
Robinwithu
Senior Contributor I

Hi Kevin,

can you mail me your project (Code) i can compile here , having CW 10.5  and PE USB Multilink Interface programming Hardware.

Thanks and Regards,

Robin

0 Kudos
Reply

1,929 Views
Robinwithu
Senior Contributor I

Hi Kevin,

May be this is useful for you ,please go through it.

CW10.5 debug problem &gt; Cannot enter background mode. Check connections.

Thanks and Regards,

Robin

0 Kudos
Reply