CAN_LDD Filter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN_LDD Filter

Jump to solution
3,969 Views
CCandido
Contributor V

Hi,

my teste bus with 10 IDs.

how to set filter to: read 3 ID/10 ID?

ex:

read ID: 0x7E0,0x7E1,0x7E2, others IDs not read.

500khz, interval between frames = 90uS.

how to  ISR use filter for the ID must read.

simple cmp not have timer!

if(  ID == ID[i] )

save

else

not save

my test with  K70.

thanks

Carlos.

0 Kudos
Reply
1 Solution
3,651 Views
CCandido
Contributor V

Hi Zhou,

thank you for your help.

Solved Invidual acceptance mask filter.

see:

Can_filter_ok.jpg

calc_id_mask

uint mask   = your_id ;   // 0001-1111-1111-1100-0000-0000-0000-0000

   mask  = mask << 18;

   mask |= 0x3FFFF;  < ---Acceptance mask invidual

//-----------------------------------------

void CAN1_OnFullRxBuffer(LDD_TUserData *UserDataPtr, LDD_CAN_TMBIndex BufferIdx)

{

simple

    switch(  BufferIdx){ read buffer_x }

}

//-----------------------------------

Thanks,

Carlos.

View solution in original post

0 Kudos
Reply
5 Replies
3,651 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Carlos candido,

    Thank you for your more information.

     I already help you create a K70 KDS CAN_LDD project, you can refer to my project, the CAN_LDD configuration is like following:

71.jpg

Because you want to receive the standard ID:0x7E0,0x7E1,0x7E2

the standard ID is 11bit, it is:

0x7e0: 11111100000

0x7e1: 11111100001

0x7e2: 11111100010

Then, you can use the acceptance mask to care all the higher 9 bit ID, and don't care the lower 2bit.

so you can configure the acceptance mask for buff(register CAN1_RXMGMASK) = 0x1ff3ffff, you can combine the Rx FIFO structure in RM to understand it:

72.jpg

Actually, if you don't care the lower 2 bit of the standard ID, you can receive just 0x7E0,0x7E1,0x7E2, 0x7e3, then all other standard ID won't be received.

I already test my project on my TWR-K70F120M, the test result is like following:

70.jpg

You will find 0x7E0,0x7E1,0x7E2 can be received by the K70, but the 0X123 will be reject.

More details, please refer to my attached project.

Wish it helps you!

If you still have question, please let me know!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,651 Views
CCandido
Contributor V

Hi Zhou,

thank you for your help.

Mode : 1

Golbal Acceptance Mask, Buffer 0...N = ok

Mode :2

Invidual Accptance Mask = not run all ID

see:

my_function_calc_mask()

{

uint mask   = 0x7C4;

uint xor      = 0x1FFFFFFF;

uint accep = 0x1FFFFFF; // 0001-1111-1111-1100-0000-0000-0000-0000

            mask  = mask << 18;

            mask |= 0x3FFFF;  < ---Acceptance mask ividual

}

CAN_Invidual Mak.jpg

note:

Buffer:0 0x7C1 = ok

Buffer:2 0x7C2 =  not accepted

Buffer:3 0x7C3 = ok

Buffer:4 0x7C4 = not accepted

buffer_zero defined all masks.

thanks,

Carlos.

0 Kudos
Reply
3,652 Views
CCandido
Contributor V

Hi Zhou,

thank you for your help.

Solved Invidual acceptance mask filter.

see:

Can_filter_ok.jpg

calc_id_mask

uint mask   = your_id ;   // 0001-1111-1111-1100-0000-0000-0000-0000

   mask  = mask << 18;

   mask |= 0x3FFFF;  < ---Acceptance mask invidual

//-----------------------------------------

void CAN1_OnFullRxBuffer(LDD_TUserData *UserDataPtr, LDD_CAN_TMBIndex BufferIdx)

{

simple

    switch(  BufferIdx){ read buffer_x }

}

//-----------------------------------

Thanks,

Carlos.

0 Kudos
Reply
3,651 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Carlos candido,

   Please tell me which IDE you are using? and the ID type is standard or extend ID?

Waiting for your reply!

Jingjing

0 Kudos
Reply
3,651 Views
CCandido
Contributor V

Hi Zhou,

I use IDE KDS30.

Type ID Stander.

Twr-K70F.

Thanks

Carlos

0 Kudos
Reply