C_CAN, FLEXCAN and MSCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

C_CAN, FLEXCAN and MSCAN

2,941件の閲覧回数
SecondTechCo
Contributor IV

WHats is the difference between C_CAN, FLEXCAN and MSCAN.  I have code eirttenr for MSCAN ?  will i have to rewrite it for FLEXCAN

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

2,753件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi William Nicholson,

   MSCAN mainly from KE and KEA series, it is the simple CAN module, this is the MSCAN bock:

pastedImage_1.png

   FlexCAN is the enhanced CAN module, it is a little complex than the MSCAN, these two CAN module have different structure.

pastedImage_2.png

About CCAN, I don't know where you find it, you can check that module datasheet to find the details.

What's the kinetis chip you are using now? KV? If yes, you need to use the flexCAN, the code you can refer to the SDK code which can be downloaded from this link:

Welcome | MCUXpresso SDK Builder 


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信