Backup reset (kinetics KE04)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Backup reset (kinetics KE04)

ソリューションへジャンプ
2,235件の閲覧回数
jun1
Contributor V

Hi.

Does the WDT reset stand in the status register when the backup reset function works and is reset? SIM_SRSID [WDOG]

thank you.

 

jun.

 

0 件の賞賛
返信
1 解決策
2,211件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

SIM_SRSID [WDOG] will stand when system reset by backup reset.

nxf58904_0-1600146959150.png

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,212件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

SIM_SRSID [WDOG] will stand when system reset by backup reset.

nxf58904_0-1600146959150.png

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,206件の閲覧回数
jun1
Contributor V

Thank you very much.

jun.

0 件の賞賛
返信