Backup reset (kinetics KE04)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Backup reset (kinetics KE04)

跳至解决方案
1,586 次查看
jun1
Contributor V

Hi.

Does the WDT reset stand in the status register when the backup reset function works and is reset? SIM_SRSID [WDOG]

thank you.

 

jun.

 

0 项奖励
回复
1 解答
1,562 次查看
nxf58904
NXP Employee
NXP Employee

Hi,

SIM_SRSID [WDOG] will stand when system reset by backup reset.

nxf58904_0-1600146959150.png

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,563 次查看
nxf58904
NXP Employee
NXP Employee

Hi,

SIM_SRSID [WDOG] will stand when system reset by backup reset.

nxf58904_0-1600146959150.png

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,557 次查看
jun1
Contributor V

Thank you very much.

jun.

0 项奖励
回复