BSDL file for MK24FN1M0VLL12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BSDL file for MK24FN1M0VLL12

跳至解决方案
620 次查看
amedrano95
Contributor I

Hello, 

Where can I find the BSDL for this IC?

0 项奖励
回复
1 解答
606 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @amedrano95 ,

Thanks for your post. Regarding the BSDL file for MK24FN1M0VLL12, you can locate it at https://www.nxp.com/webapp/Download?colCode=K64_K63_K24_BSDL . MK24FN1M0VLL12 comes in the LQFP100 package, and the file named K24_100qfp.bsdl is the one you need.

Celeste_Liu_0-1736216604173.png

 

Hope it can help you.

BRs,

Celeste

 

--------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
--------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
607 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @amedrano95 ,

Thanks for your post. Regarding the BSDL file for MK24FN1M0VLL12, you can locate it at https://www.nxp.com/webapp/Download?colCode=K64_K63_K24_BSDL . MK24FN1M0VLL12 comes in the LQFP100 package, and the file named K24_100qfp.bsdl is the one you need.

Celeste_Liu_0-1736216604173.png

 

Hope it can help you.

BRs,

Celeste

 

--------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
--------------------------------------------------------------------------------------------------------

0 项奖励
回复