Are the MK2 UART_RX pins 5V tolerant

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are the MK2 UART_RX pins 5V tolerant

ソリューションへジャンプ
2,097件の閲覧回数
patrickirwin
Contributor I

Hello,

I have a question about the MK26FN2M0VMI18.  Are the UART_RX pins 5V tolerant? 

I have taken over a design from an engineer that has left our company.  And he has a 5V RS485 signal going to an UART_RX pin. 

I do not see in the datasheet that this pin is 5V tolerant. 

Thanks,

Pat

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,090件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Pat,

Sorry for the inconvenience we bring you!
IO on MK26 are not 5V tolerant.
Part numbers that support 5V tolerant will be mentioned in the Data Sheet.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,091件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Pat,

Sorry for the inconvenience we bring you!
IO on MK26 are not 5V tolerant.
Part numbers that support 5V tolerant will be mentioned in the Data Sheet.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信