Are the MK2 UART_RX pins 5V tolerant

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Are the MK2 UART_RX pins 5V tolerant

跳至解决方案
2,096 次查看
patrickirwin
Contributor I

Hello,

I have a question about the MK26FN2M0VMI18.  Are the UART_RX pins 5V tolerant? 

I have taken over a design from an engineer that has left our company.  And he has a 5V RS485 signal going to an UART_RX pin. 

I do not see in the datasheet that this pin is 5V tolerant. 

Thanks,

Pat

 

标签 (1)
0 项奖励
回复
1 解答
2,089 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Pat,

Sorry for the inconvenience we bring you!
IO on MK26 are not 5V tolerant.
Part numbers that support 5V tolerant will be mentioned in the Data Sheet.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,090 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Pat,

Sorry for the inconvenience we bring you!
IO on MK26 are not 5V tolerant.
Part numbers that support 5V tolerant will be mentioned in the Data Sheet.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复