Are the MK2 UART_RX pins 5V tolerant

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are the MK2 UART_RX pins 5V tolerant

Jump to solution
2,098 Views
patrickirwin
Contributor I

Hello,

I have a question about the MK26FN2M0VMI18.  Are the UART_RX pins 5V tolerant? 

I have taken over a design from an engineer that has left our company.  And he has a 5V RS485 signal going to an UART_RX pin. 

I do not see in the datasheet that this pin is 5V tolerant. 

Thanks,

Pat

 

Labels (1)
0 Kudos
Reply
1 Solution
2,091 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Pat,

Sorry for the inconvenience we bring you!
IO on MK26 are not 5V tolerant.
Part numbers that support 5V tolerant will be mentioned in the Data Sheet.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,092 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Pat,

Sorry for the inconvenience we bring you!
IO on MK26 are not 5V tolerant.
Part numbers that support 5V tolerant will be mentioned in the Data Sheet.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply