Another question regarding PK and MK devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Another question regarding PK and MK devices

ソリューションへジャンプ
2,355件の閲覧回数
georgschmidt
Contributor III

Hi,

on my current PCB I am running a MK61FX512VMD12 controller with maskset 3N96B and date code 12/50.
Now I got offered a number of PK61FX512VMD12 controllers with the same maskset and date code 13/38. Please see the attached pictures.
Can I assume the code that runs on the MK devices will run also on the PK devices without any modification?

Regards,
Georg

MK61.jpg

PK61.jpg

  

0 件の賞賛
返信
1 解決策
2,350件の閲覧回数
jay_heng
NXP Employee
NXP Employee

PK part is factory sample, it is not trimmed (internal backdoor otp setting of analog module).

MK part is the final chip for customer.

From digital peripheral point of view, PK part is same as MK part.

元の投稿で解決策を見る

2 返答(返信)
2,346件の閲覧回数
georgschmidt
Contributor III

Thanks for your reply!

0 件の賞賛
返信
2,351件の閲覧回数
jay_heng
NXP Employee
NXP Employee

PK part is factory sample, it is not trimmed (internal backdoor otp setting of analog module).

MK part is the final chip for customer.

From digital peripheral point of view, PK part is same as MK part.