After flashing the code for the first time, Micro receives Lock MKE14F512VLL16.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

After flashing the code for the first time, Micro receives Lock MKE14F512VLL16.

ソリューションへジャンプ
2,555件の閲覧回数
pratik_s_khule
Contributor I

Hi Team,

I'm working on a Kinetis KE14F512VLL16 Microcontroller.

After flashing the code for the first time, the microcontroller becomes locked.

I couldn't flash the code or delete the memory after that.

I'm using J-link SEGGER and IAR Embedded Workbench IDE - ARM 8.32.4, and I've tried J-FLASH as well.

 

pratik_s_khule_0-1652442063251.png

because of the micro lock When I try to programmed again, I get the following error:

pratik_s_khule_1-1652448736756.png

Could you please assist me in resolving this problem?

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,541件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi pratik_s_khule,

Please refer the "Figure 36. Reset circuit" and "Figure 38. NMI pin biasing" and "Figure 39. SWD debug interface" of Kinetis KE1xF with up to 512 KB Flash

6.1.4 Digital design.png

Then refer the methods descripted in: Communication error while accessing MDM-AP.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,542件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi pratik_s_khule,

Please refer the "Figure 36. Reset circuit" and "Figure 38. NMI pin biasing" and "Figure 39. SWD debug interface" of Kinetis KE1xF with up to 512 KB Flash

6.1.4 Digital design.png

Then refer the methods descripted in: Communication error while accessing MDM-AP.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------