After flashing the code for the first time, Micro receives Lock MKE14F512VLL16.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

After flashing the code for the first time, Micro receives Lock MKE14F512VLL16.

跳至解决方案
1,782 次查看
pratik_s_khule
Contributor I

Hi Team,

I'm working on a Kinetis KE14F512VLL16 Microcontroller.

After flashing the code for the first time, the microcontroller becomes locked.

I couldn't flash the code or delete the memory after that.

I'm using J-link SEGGER and IAR Embedded Workbench IDE - ARM 8.32.4, and I've tried J-FLASH as well.

 

pratik_s_khule_0-1652442063251.png

because of the micro lock When I try to programmed again, I get the following error:

pratik_s_khule_1-1652448736756.png

Could you please assist me in resolving this problem?

 

标签 (1)
0 项奖励
回复
1 解答
1,768 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi pratik_s_khule,

Please refer the "Figure 36. Reset circuit" and "Figure 38. NMI pin biasing" and "Figure 39. SWD debug interface" of Kinetis KE1xF with up to 512 KB Flash

6.1.4 Digital design.png

Then refer the methods descripted in: Communication error while accessing MDM-AP.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,769 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi pratik_s_khule,

Please refer the "Figure 36. Reset circuit" and "Figure 38. NMI pin biasing" and "Figure 39. SWD debug interface" of Kinetis KE1xF with up to 512 KB Flash

6.1.4 Digital design.png

Then refer the methods descripted in: Communication error while accessing MDM-AP.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------