About sleep current in STOP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About sleep current in STOP mode

1,323件の閲覧回数
Sourdev
Contributor II

I am using the S9KEAZN64AMLC microcontroller. I put the device into STOP mode using wfi() instructions. In stop mode, MCU consumes 130uA with a supply voltage of 5V.

In the datasheet, it is mentioned that the stop current is 2uA.

Sourdev_0-1683896618445.pngSourdev_0-1683896618445.png

How I will get 2uA current?

0 件の賞賛
返信
1 返信

1,297件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Sourdev,

Do you use the NXP development board to test, or test the circuit board designed by yourself? 

If you are using FRDM-KEAZN32 board, since the convenience of low-power testing is not considered, I am afraid you have to remove several external resistors to get the correct current consumption. You can refer to the discussion in how to achieve the KEA128 lowest static current in STOP mode

If you use circuit board designed by yourself, then please check the external circuit to avoid those case:

Fig3_internalpullupdowncell.JPGFig3_internalpullupdowncell.JPG


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信