About KE04 glitch filter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About KE04 glitch filter

Jump to solution
2,691 Views
jun1
Contributor V

Thank you for your help.

KE04 Subfamily Reference Manual, Rev. 4, 01/2019
The 11.4 input glitch filter settings were written as follows:

Glitches that are shorter than the selected clock period will be filtered out; Glitches that are more than twice the selected clock period will not be filtered out. It will pass to internal circuitry.

I have a question here,
Are glitches longer than the selected clock period and less than twice the period removed?
Do I have to think like the attached diagram?

Thank you.

jun.

Labels (1)
0 Kudos
Reply
1 Solution
2,536 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi jun,

The result of filtering glitch between one clock and two clock is not certain. Sometime it can pass, and sometime it can't.  This is determined by the time of sampling edge. If it can be sampled by 2 edge, it can pass. Your picture is correct.

Regards,

Jing

View solution in original post

0 Kudos
Reply
2 Replies
2,536 Views
jun1
Contributor V

Hi.

Thank you very much for your kindness. I understand that.

jun.

0 Kudos
Reply
2,537 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi jun,

The result of filtering glitch between one clock and two clock is not certain. Sometime it can pass, and sometime it can't.  This is determined by the time of sampling edge. If it can be sampled by 2 edge, it can pass. Your picture is correct.

Regards,

Jing

0 Kudos
Reply