pre loaded code not running after power on using kinetis design studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pre loaded code not running after power on using kinetis design studio

882 Views
lijofrancis
Contributor III

Dear sir,

I am using Kinetis Design studio 2.0 with update,and we use K60 towerboard.i load the code using the mode debug as....its working....

my code running successfully......

But my problem is that after i power off the tower board then power on ,the code not running.......

is that code load into ram ? not flash?....

why that code not running after power restart?

How the  code, we loaded has gone?

 

 

in KDS we checked flash from file that not working.....................................

programmer we use Pe Micro....please tell me how to resolve my problem

Please tell me its very urgent

Labels (1)
0 Kudos
Reply
1 Reply

791 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Lijo,

I recommend you first test on simple project , please see the attachment,  it is create on TWR-K60D10M board,

and the function of the project is light the LED , please download  it , and the power off , then power on to test .

I have test it on my side ,it can work well when re-power on.

Hope it helps

Alice

0 Kudos
Reply