pre loaded code not running after power on using kinetis design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pre loaded code not running after power on using kinetis design studio

1,264件の閲覧回数
lijofrancis
Contributor III

Dear sir,

I am using Kinetis Design studio 2.0 with update,and we use K60 towerboard.i load the code using the mode debug as....its working....

my code running successfully......

But my problem is that after i power off the tower board then power on ,the code not running.......

is that code load into ram ? not flash?....

why that code not running after power restart?

How the  code, we loaded has gone?

 

 

in KDS we checked flash from file that not working.....................................

programmer we use Pe Micro....please tell me how to resolve my problem

Please tell me its very urgent

ラベル(1)
0 件の賞賛
返信
1 返信

1,173件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Lijo,

I recommend you first test on simple project , please see the attachment,  it is create on TWR-K60D10M board,

and the function of the project is light the LED , please download  it , and the power off , then power on to test .

I have test it on my side ,it can work well when re-power on.

Hope it helps

Alice

0 件の賞賛
返信