openocd error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

openocd error

1,492件の閲覧回数
martinfiset
Contributor I

Board:     FRDM-K22F rev A1

IDE:     KDS v3.2.0

Firnware version:     0203

                                   And I upgraded to 0221 a few minutes ago  (I upgraded to 0221_k20dx128_k22f_0x8000.bin)

SDK:     v2.0 for FRDM-K22F

 

Two weeks ago I was successfull in debugging the "Hello World" example on the FRDM-K22F using OpenOCD debugging.

Today I receive errors when trying to debbug the "Hello World" example.

 

Here is what OpenOCD gives:

For bug reports, read   http://openocd.sourceforge.net/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'cmsis-dap'

Error: unable to open CMSIS-DAP device

Error: unable to init CMSIS-DAP driver

Error: Error selecting 'cmsis-dap' as transport

Runtime Error: C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg:3:

in procedure 'script'

at file "embedded:startup.tcl", line 58

in procedure 'interface' called at file "C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg", line 3

 

And here is the error I receive from the debugger in Eclipse:

146592_146592.pngpastedImage_3.png

I did observe this with the original firmware version 203. Then I upgraded to version 221, but still the error is the same.

I made sure I had the "-f kinetis.cfg" in the debugger config options. Still the same error.

 

I tried running the openocd command line executable. Here is what happended:

146593_146593.pngpastedImage_5.png

It seems the device is secured.

But the only thing I did with the board was debugging the "Hello World" example two weeks ago, and then today I am ready to start development, and I am unable to run the "Hello World" example.

 

Any hint?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,018件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I would suggest you try J-link OpenSDA or P&E OpenSDA, see how it works with this board.

please follow this article to update the firmware and check board connection:

Summary of FRDM-K22F debug interface

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信