kinetis-design-studio_3.2.0 install failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

kinetis-design-studio_3.2.0 install failed

跳至解决方案
1,615 次查看
felixzhu
Contributor I

Installation of kinetis-design-studio_3.2.0 is failed on Windows 10 home edition.

log file is attached.

Any suggestion?

Original Attachment has been moved to: MSIb38.LOG.zip

标签 (1)
0 项奖励
回复
1 解答
1,445 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

kinetis-design-studio_3.2.0 is designed for Windows® 7/8/10 (32 and 64-bit). so user can install it on win10 without problem.

during install, please make sure you have windows admin right. this is important.

during install, please disable all the virus defender and firewall. this may prevent install process working.

if the install still fails, please post the error screenshot here. this may help us shoot the trouble. thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,446 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

kinetis-design-studio_3.2.0 is designed for Windows® 7/8/10 (32 and 64-bit). so user can install it on win10 without problem.

during install, please make sure you have windows admin right. this is important.

during install, please disable all the virus defender and firewall. this may prevent install process working.

if the install still fails, please post the error screenshot here. this may help us shoot the trouble. thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------