kinetis-design-studio_3.2.0 install failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kinetis-design-studio_3.2.0 install failed

ソリューションへジャンプ
1,607件の閲覧回数
felixzhu
Contributor I

Installation of kinetis-design-studio_3.2.0 is failed on Windows 10 home edition.

log file is attached.

Any suggestion?

Original Attachment has been moved to: MSIb38.LOG.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
1,437件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

kinetis-design-studio_3.2.0 is designed for Windows® 7/8/10 (32 and 64-bit). so user can install it on win10 without problem.

during install, please make sure you have windows admin right. this is important.

during install, please disable all the virus defender and firewall. this may prevent install process working.

if the install still fails, please post the error screenshot here. this may help us shoot the trouble. thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,438件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

kinetis-design-studio_3.2.0 is designed for Windows® 7/8/10 (32 and 64-bit). so user can install it on win10 without problem.

during install, please make sure you have windows admin right. this is important.

during install, please disable all the virus defender and firewall. this may prevent install process working.

if the install still fails, please post the error screenshot here. this may help us shoot the trouble. thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------