kinetis-design-studio_3.2.0 install failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kinetis-design-studio_3.2.0 install failed

Jump to solution
1,584 Views
felixzhu
Contributor I

Installation of kinetis-design-studio_3.2.0 is failed on Windows 10 home edition.

log file is attached.

Any suggestion?

Original Attachment has been moved to: MSIb38.LOG.zip

Labels (1)
0 Kudos
Reply
1 Solution
1,414 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

kinetis-design-studio_3.2.0 is designed for Windows® 7/8/10 (32 and 64-bit). so user can install it on win10 without problem.

during install, please make sure you have windows admin right. this is important.

during install, please disable all the virus defender and firewall. this may prevent install process working.

if the install still fails, please post the error screenshot here. this may help us shoot the trouble. thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,415 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

kinetis-design-studio_3.2.0 is designed for Windows® 7/8/10 (32 and 64-bit). so user can install it on win10 without problem.

during install, please make sure you have windows admin right. this is important.

during install, please disable all the virus defender and firewall. this may prevent install process working.

if the install still fails, please post the error screenshot here. this may help us shoot the trouble. thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------