debug frdm-k82f

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

debug frdm-k82f

4,113件の閲覧回数
mesdouaabderraz
Contributor III

hi i encounter a problem when i  trail to debug a project withe frdm-k82f , any help please?Capture.PNG?

5 返答(返信)

3,851件の閲覧回数
harshpatel
Contributor IV

H‌ello MESDOUA Abderrazek

Nxp guys Alice_Yang can help in this issue.  

Regards

Harsh Patel

0 件の賞賛
返信

3,851件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mesdoua,

- Please update the firmware use the attachment "04_OpenSDA_FRDM-K82F.bin",

the steps as below :

1)Press the Reset button (and keep it pressed) while power the board with the OpenSDA USB connector(J5):.
2)  The board will show up as BOOTLOADER drive on your system:
3) Copy"04_OpenSDA_FRDM-K82F.bin" to the BOOTLOADER driver:
4) The copy operation takes about 2-3 seconds, after finished , un power the board.
5) Power the board again normally .

- Then configure the debug view as Harsh Patel mentioned .

If still can't work, please take a video  or screenshot to show your steps.

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,849件の閲覧回数
harshpatel
Contributor IV

Hello   MESDOUA Abderrazek

 Need some more detail to find issue but make sure following three things:

1]  Enter your correct device name in debug configuration as shown in attachment

2]  Make sure J-link and frdm board are 1 to 1 connected properly using Cable.

 3] J link is Powered On properly

Let me know if any..

Regards

Harsh Patel

3,849件の閲覧回数
mesdouaabderraz
Contributor III

hi, thank you for your answer, i just have a question if it's possible please :

There is an example who can help me or a demo folder over uart connection?

because on my project i had buy a frdm-k82f nxp board and a Fingerprint Scanner GT-511C1R, and i want to connect they with uart port TX RX like on picture , for realise a test of Fingerprint recognition,

i know that i must write a code but my question is, There is an example who can help me or a demo folder on this topic?1.PNG

0 件の賞賛
返信

3,849件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mesdoua,

About the UART example, you find in MCUXpresso SDK,  about how to download please refer to :

https://community.nxp.com/docs/DOC-333304 

Sorry I don't know the GT-511C1R  clealy.

BR

Alice

0 件の賞賛
返信