compile with linker only

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

compile with linker only

跳至解决方案
2,164 次查看
roymessinger
Contributor V

when making changes to linker file only, then compiling, the KDS disregards the linker changes. Only after cleaning the project does the KDS look at the linker file (obviously also compiling all the rest, taking time).

I want to make changes to the linker file only and compile without the hassle to clean project and compile all files.. 

How can I do that?

1 解答
2,015 次查看
BlackNight
NXP Employee
NXP Employee

Hi Roy,

yes, a linker file change does not trigger a new link. This is (imho) a problem of the GNU ARM → GNU MCU Eclipse!  plugins. I have reported that a while back, but to my knowledge it is still not changed in the latest version of the plugins. But it could be a CDT problem too.

What I usually do is to touch/change a source file to trigger a link phase.

I hope this helps,

Erich

在原帖中查看解决方案

1 回复
2,016 次查看
BlackNight
NXP Employee
NXP Employee

Hi Roy,

yes, a linker file change does not trigger a new link. This is (imho) a problem of the GNU ARM → GNU MCU Eclipse!  plugins. I have reported that a while back, but to my knowledge it is still not changed in the latest version of the plugins. But it could be a CDT problem too.

What I usually do is to touch/change a source file to trigger a link phase.

I hope this helps,

Erich