Why I can't read register values ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why I can't read register values ?

2,747 Views
nadiajarray
Contributor II

I have added register detail view in KDS like mentioned here https://mcuoneclipse.com/2014/05/29/how-to-add-register-details-view-in-eclipse/ but during debugging when I double click the register it turns out green but no value appears.

154401_154401.pngextint1.png

What I'm doing wrong here plz ?

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,232 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Nadia,

Which version of KDS do you used?

I recommend you use the latest version of KDS v3.2 , we can directly check the register without

install anything .

You can download and install it refer to this :

New Kinetis Design Studio v3.2.0 available

Also in the "EmbSys Registers" view to check the registers .

pastedImage_1.png

You can find this view on "Window -> show View->......" :

pastedImage_2.png

pastedImage_3.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,231 Views
nadiajarray
Contributor II

I'm using already the KDS V3.2

0 Kudos
Reply

2,232 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

The KDS v3.2 needn't install anything when read register .

Double click the register which you want to check , it can show the data :

pastedImage_0.png

If you have install the Embsys Registers again refer to the thread you mentioned , i recommend

you uninstall the KDS , then install it again .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply