Usage of function RxCallback for fsl_uart component

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Usage of function RxCallback for fsl_uart component

1,276件の閲覧回数
sergiosaucedo
Contributor I

I'm new in KDS and Kinetis FRDM, but I wanna use a interruption for receive data from UART.

I'm using fsl_uart component whit the Rx configuration in the image.

Can someone tell me, how and when is the UART_RxCallback(uint32_t instance, void * uartState) works?

or if I can use it as interrupt for mi program?.

152850_152850.pngpastedImage_0.png

ラベル(1)
0 件の賞賛
返信
1 返信

1,072件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

see this thread

How can I use RxCallback for fsl_uart component


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信