The program is bouncing in KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The program is bouncing in KDS

1,766 次查看
jinhuiwu
Contributor II

in source code ,it is a for cycle.but in the assembler,"MotorBoard_State=SELFTESTING1"insert.

I don't use OS,it is very strange.

Is this kds's bug?

555133149318922450.jpg137258985078116783.jpg

0 项奖励
回复
4 回复数

1,630 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Could you describe your question more detail ?

When run these code, what error does it shows ?

BR

Alice

0 项奖励
回复

1,630 次查看
jinhuiwu
Contributor II

The PC point jump at 1161 from 43.

0 项奖励
回复

1,630 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jinhui,

Please clean your project, also delete the file of intermediate files :

pastedImage_1.png

then rebuild to test again. If still have this error, pleas search where is the

code in your project, this is link to wrong place,  if you can't find it , please

share your project to me .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,630 次查看
jinhuiwu
Contributor II

very thanks ,I am trying

0 项奖励
回复