The program is bouncing in KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The program is bouncing in KDS

2,391件の閲覧回数
jinhuiwu
Contributor II

in source code ,it is a for cycle.but in the assembler,"MotorBoard_State=SELFTESTING1"insert.

I don't use OS,it is very strange.

Is this kds's bug?

555133149318922450.jpg137258985078116783.jpg

0 件の賞賛
返信
4 返答(返信)

2,255件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Could you describe your question more detail ?

When run these code, what error does it shows ?

BR

Alice

0 件の賞賛
返信

2,255件の閲覧回数
jinhuiwu
Contributor II

The PC point jump at 1161 from 43.

0 件の賞賛
返信

2,255件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jinhui,

Please clean your project, also delete the file of intermediate files :

pastedImage_1.png

then rebuild to test again. If still have this error, pleas search where is the

code in your project, this is link to wrong place,  if you can't find it , please

share your project to me .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,255件の閲覧回数
jinhuiwu
Contributor II

very thanks ,I am trying

0 件の賞賛
返信