Alice,
I guess I am wrong, In the first screen shot attached I have selected the PCS0,1,2 however in the chip select configurations I have selected the SPI0_PCS0, 2 and 3. but not SPI0_PCS1.
My slaves devices are connected on SPI0_PCS0, SPI0_PC2, SPI0_PCS3 so I should be selecteding the Masterconfig with PCS0, PCS2, PCS3 right.
so by doing that and what you suggested doing an external init I am able to get a response from PCS2 and PCS3. but failed to get any response from PCS0 however, the PCS0 enable is going low. So is it that the MISO line is held low/ high impedance state by any other devices.

I am doing an external SPI Initialize using code below just before sending the first packet.
void InitializeSPI( void )
{
// /* SIM_SCGC6: SPI0=1 */
// SIM_SCGC6 |= SIM_SCGC6_SPI0_MASK;
// /* Interrupt vector(s) priority setting */
//// /* NVICIP26: PRI26=0x70 */
//// NVICIP26 = NVIC_IP_PRI26(0x70);
//// /* NVICISER0: SETENA|=0x04000000 */
//// NVICISER0 |= NVIC_ISER_SETENA(0x04000000);
// /* SIM_SCGC5: PORTD=1 */
// SIM_SCGC5 |= SIM_SCGC5_PORTD_MASK;
// /* PORTD_PCR3: ISF=0,MUX=2 */
// PORTD_PCR3 = (uint32_t)((PORTD_PCR3 & (uint32_t)~(uint32_t)(
// PORT_PCR_ISF_MASK |
// PORT_PCR_MUX(0x05)
// )) | (uint32_t)(
// PORT_PCR_MUX(0x02)
// ));
// /* PORTD_PCR2: ISF=0,MUX=2 */
// PORTD_PCR2 = (uint32_t)((PORTD_PCR2 & (uint32_t)~(uint32_t)(
// PORT_PCR_ISF_MASK |
// PORT_PCR_MUX(0x05)
// )) | (uint32_t)(
// PORT_PCR_MUX(0x02)
// ));
// /* PORTD_PCR1: ISF=0,MUX=2 */
// PORTD_PCR1 = (uint32_t)((PORTD_PCR1 & (uint32_t)~(uint32_t)(
// PORT_PCR_ISF_MASK |
// PORT_PCR_MUX(0x05)
// )) | (uint32_t)(
// PORT_PCR_MUX(0x02)
// ));
// /* PORTD_PCR4: ISF=0,MUX=2 */
// PORTD_PCR4 = (uint32_t)((PORTD_PCR4 & (uint32_t)~(uint32_t)(
// PORT_PCR_ISF_MASK |
// PORT_PCR_MUX(0x05)
// )) | (uint32_t)(
// PORT_PCR_MUX(0x02)
// ));
// /* PORTD_PCR5: ISF=0,MUX=2 */
// PORTD_PCR5 = (uint32_t)((PORTD_PCR5 & (uint32_t)~(uint32_t)(
// PORT_PCR_ISF_MASK |
// PORT_PCR_MUX(0x05)
// )) | (uint32_t)(
// PORT_PCR_MUX(0x02)
// ));
// /* PORTD_PCR0: ISF=0,MUX=2 */
// PORTD_PCR0 = (uint32_t)((PORTD_PCR0 & (uint32_t)~(uint32_t)(
// PORT_PCR_ISF_MASK |
// PORT_PCR_MUX(0x05)
// )) | (uint32_t)(
// PORT_PCR_MUX(0x02)
// ));
// /* PORTD_PCR6: ISF=0,MUX=2 */
// PORTD_PCR6 = (uint32_t)((PORTD_PCR6 & (uint32_t)~(uint32_t)(
// PORT_PCR_ISF_MASK |
// PORT_PCR_MUX(0x05)
// )) | (uint32_t)(
// PORT_PCR_MUX(0x02)
// ));
/* SPI0_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=1,??=0,??=0,PCSIS=0x0F,DOZE=0,MDIS=0,DIS_TXF=0,DIS_RXF=0,CLR_TXF=0,CLR_RXF=0,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */
SPI0_MCR = SPI_MCR_DCONF(0x00) |
SPI_MCR_ROOE_MASK |
SPI_MCR_PCSIS(0x0F) |
SPI_MCR_SMPL_PT(0x00) |
SPI_MCR_HALT_MASK; /* Set Configuration register */
/* SPI0_MCR: MSTR=1,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=1,??=0,??=0,PCSIS=0x0F,DOZE=0,MDIS=0,DIS_TXF=1,DIS_RXF=1,CLR_TXF=1,CLR_RXF=1,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */
SPI0_MCR = SPI_MCR_MSTR_MASK |
SPI_MCR_DCONF(0x00) |
SPI_MCR_ROOE_MASK |
SPI_MCR_PCSIS(0x0F) |
SPI_MCR_DIS_TXF_MASK |
SPI_MCR_DIS_RXF_MASK |
SPI_MCR_CLR_TXF_MASK |
SPI_MCR_CLR_RXF_MASK |
SPI_MCR_SMPL_PT(0x00) |
SPI_MCR_HALT_MASK; /* Set Configuration register */
/* SPI0_CTAR0: DBR=1,FMSZ=0x0F,CPOL=0,CPHA=0,LSBFE=0,PCSSCK=3,PASC=3,PDT=3,PBR=2,CSSCK=1,ASC=1,DT=1,BR=1 */
SPI0_CTAR0 = SPI_CTAR_DBR_MASK |
SPI_CTAR_FMSZ(0x07) |
SPI_CTAR_PCSSCK(0x03) |
SPI_CTAR_PASC(0x03) |
SPI_CTAR_PDT(0x03) |
SPI_CTAR_PBR(0x02) |
SPI_CTAR_CSSCK(0x01) |
SPI_CTAR_ASC(0x01) |
SPI_CTAR_DT(0x01) |
SPI_CTAR_BR(0x01); /* Set Clock and Transfer Attributes register */
/* SPI0_SR: TCF=1,TXRXS=0,??=0,EOQF=1,TFUF=1,??=0,TFFF=1,??=0,??=0,??=0,??=1,??=0,RFOF=1,??=0,RFDF=1,??=0,TXCTR=0,TXNXTPTR=0,RXCTR=0,POPNXTPTR=0 */
SPI0_SR = SPI_SR_TCF_MASK |
SPI_SR_EOQF_MASK |
SPI_SR_TFUF_MASK |
SPI_SR_TFFF_MASK |
SPI_SR_RFOF_MASK |
SPI_SR_RFDF_MASK |
SPI_SR_TXCTR(0x00) |
SPI_SR_TXNXTPTR(0x00) |
SPI_SR_RXCTR(0x00) |
SPI_SR_POPNXTPTR(0x00) |
0x00200000U; /* Clear flags */
/* SPI0_RSER: TCF_RE=0,??=0,??=0,EOQF_RE=0,TFUF_RE=0,??=0,TFFF_RE=0,TFFF_DIRS=0,??=0,??=0,??=0,??=0,RFOF_RE=0,??=0,RFDF_RE=1,RFDF_DIRS=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
SPI0_RSER = SPI_RSER_RFDF_RE_MASK; /* Set DMA Interrupt Request Select and Enable register */
/* SPI0_MCR: HALT=0 */
SPI0_MCR &= (uint32_t)~(uint32_t)(SPI_MCR_HALT_MASK);
}