SPI Chip select and configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Chip select and configuration

Jump to solution
5,783 Views
Kewal
Contributor IV

Hi,

 

I have an SPI master(K64) configured with below settings. Currently, I am able to communicate only with one of the slave connected on Chip select pin PTD6. I am not doing anything through code apart from setdelay between CS and Clock. So is there anything else which needs to be configured.

 

 

 

126955_126955.JPGSPIMasterConfiguration.JPG

 

 

 

126953_126953.JPGSPIChipselect.JPG

 

How does the HAL know which pin chip selects to, if its PTD5,6,0

 

In the HAL layer, all I could see was

 

/*! @brief DSPI Peripheral Chip Select (PCS) configuration (which PCS to configure)*/

typedef enum _dspi_which_pcs_config {

    kDspiPcs0 = 1 << 0, /*!< PCS[0] @internal gui name="PCS0" */

    kDspiPcs1 = 1 << 1, /*!< PCS[1] @internal gui name="PCS1" */

    kDspiPcs2 = 1 << 2, /*!< PCS[2] @internal gui name="PCS2" */

    kDspiPcs3 = 1 << 3, /*!< PCS[3] @internal gui name="PCS3" */

    kDspiPcs4 = 1 << 4, /*!< PCS[4] @internal gui name="PCS4" */

    kDspiPcs5 = 1 << 5  /*!< PCS[5] @internal gui name="PCS5" */

} dspi_which_pcs_config_t;

I think its a potential bug here in KDS.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
4,666 Views
Kewal
Contributor IV

Alice,

I guess I am wrong, In the first screen shot attached I have selected the PCS0,1,2 however in the chip select configurations I have selected the SPI0_PCS0, 2 and 3. but not SPI0_PCS1.

My slaves devices are connected on SPI0_PCS0, SPI0_PC2, SPI0_PCS3 so I should be selecteding the Masterconfig with PCS0, PCS2, PCS3 right.

so by doing that and what you suggested doing an external init I am able to get a response from PCS2 and PCS3. but failed to get any response from PCS0 however, the PCS0 enable is going low. So is it that the MISO line is held low/ high impedance state by any other devices.

SPI without response.JPG

I am doing an external SPI Initialize using code below just before sending the first packet.

void InitializeSPI( void )

{

//    /* SIM_SCGC6: SPI0=1 */

//  SIM_SCGC6 |= SIM_SCGC6_SPI0_MASK;

//  /* Interrupt vector(s) priority setting */

////  /* NVICIP26: PRI26=0x70 */

////  NVICIP26 = NVIC_IP_PRI26(0x70);

////  /* NVICISER0: SETENA|=0x04000000 */

////  NVICISER0 |= NVIC_ISER_SETENA(0x04000000);

//    /* SIM_SCGC5: PORTD=1 */

//  SIM_SCGC5 |= SIM_SCGC5_PORTD_MASK;

//  /* PORTD_PCR3: ISF=0,MUX=2 */

//  PORTD_PCR3 = (uint32_t)((PORTD_PCR3 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR2: ISF=0,MUX=2 */

//  PORTD_PCR2 = (uint32_t)((PORTD_PCR2 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR1: ISF=0,MUX=2 */

//  PORTD_PCR1 = (uint32_t)((PORTD_PCR1 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR4: ISF=0,MUX=2 */

//  PORTD_PCR4 = (uint32_t)((PORTD_PCR4 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR5: ISF=0,MUX=2 */

//  PORTD_PCR5 = (uint32_t)((PORTD_PCR5 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR0: ISF=0,MUX=2 */

//  PORTD_PCR0 = (uint32_t)((PORTD_PCR0 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR6: ISF=0,MUX=2 */

//  PORTD_PCR6 = (uint32_t)((PORTD_PCR6 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

  /* SPI0_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=1,??=0,??=0,PCSIS=0x0F,DOZE=0,MDIS=0,DIS_TXF=0,DIS_RXF=0,CLR_TXF=0,CLR_RXF=0,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */

  SPI0_MCR = SPI_MCR_DCONF(0x00) |

             SPI_MCR_ROOE_MASK |

             SPI_MCR_PCSIS(0x0F) |

             SPI_MCR_SMPL_PT(0x00) |

             SPI_MCR_HALT_MASK;        /* Set Configuration register */

  /* SPI0_MCR: MSTR=1,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=1,??=0,??=0,PCSIS=0x0F,DOZE=0,MDIS=0,DIS_TXF=1,DIS_RXF=1,CLR_TXF=1,CLR_RXF=1,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */

  SPI0_MCR = SPI_MCR_MSTR_MASK |

             SPI_MCR_DCONF(0x00) |

             SPI_MCR_ROOE_MASK |

             SPI_MCR_PCSIS(0x0F) |

             SPI_MCR_DIS_TXF_MASK |

             SPI_MCR_DIS_RXF_MASK |

             SPI_MCR_CLR_TXF_MASK |

             SPI_MCR_CLR_RXF_MASK |

             SPI_MCR_SMPL_PT(0x00) |

             SPI_MCR_HALT_MASK;        /* Set Configuration register */

  /* SPI0_CTAR0: DBR=1,FMSZ=0x0F,CPOL=0,CPHA=0,LSBFE=0,PCSSCK=3,PASC=3,PDT=3,PBR=2,CSSCK=1,ASC=1,DT=1,BR=1 */

  SPI0_CTAR0 = SPI_CTAR_DBR_MASK |

               SPI_CTAR_FMSZ(0x07) |

               SPI_CTAR_PCSSCK(0x03) |

               SPI_CTAR_PASC(0x03) |

               SPI_CTAR_PDT(0x03) |

               SPI_CTAR_PBR(0x02) |

               SPI_CTAR_CSSCK(0x01) |

               SPI_CTAR_ASC(0x01) |

               SPI_CTAR_DT(0x01) |

               SPI_CTAR_BR(0x01);      /* Set Clock and Transfer Attributes register */

 

 

  /* SPI0_SR: TCF=1,TXRXS=0,??=0,EOQF=1,TFUF=1,??=0,TFFF=1,??=0,??=0,??=0,??=1,??=0,RFOF=1,??=0,RFDF=1,??=0,TXCTR=0,TXNXTPTR=0,RXCTR=0,POPNXTPTR=0 */

  SPI0_SR = SPI_SR_TCF_MASK |

            SPI_SR_EOQF_MASK |

            SPI_SR_TFUF_MASK |

            SPI_SR_TFFF_MASK |

            SPI_SR_RFOF_MASK |

            SPI_SR_RFDF_MASK |

            SPI_SR_TXCTR(0x00) |

            SPI_SR_TXNXTPTR(0x00) |

            SPI_SR_RXCTR(0x00) |

            SPI_SR_POPNXTPTR(0x00) |

            0x00200000U;               /* Clear flags */

  /* SPI0_RSER: TCF_RE=0,??=0,??=0,EOQF_RE=0,TFUF_RE=0,??=0,TFFF_RE=0,TFFF_DIRS=0,??=0,??=0,??=0,??=0,RFOF_RE=0,??=0,RFDF_RE=1,RFDF_DIRS=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  SPI0_RSER = SPI_RSER_RFDF_RE_MASK;   /* Set DMA Interrupt Request Select and Enable register */

  /* SPI0_MCR: HALT=0 */

SPI0_MCR &= (uint32_t)~(uint32_t)(SPI_MCR_HALT_MASK);

}

View solution in original post

0 Kudos
Reply
4 Replies
4,666 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kewal,

Your configuration is right.

- And about which chip select to , after we configured the "chip select ", we can see the generate code on the file of"dspiCom1.c",

not on the HAL file .

pastedImage_0.png

- The reason why only one slave spi work is that, in the Auto  initialization  code ,it can only select one of them to initialize.

pastedImage_1.png

pastedImage_2.png

so  when you want select the other two slave SPI ,you can initialize them by hand refer to   the code under "comopnents_init".

or i think you can also use this function :

  DSPI_HAL_SetPcsPolarityMode(base, userConfig->whichPcs, userConfig->pcsPolarity);

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,667 Views
Kewal
Contributor IV

Alice,

I guess I am wrong, In the first screen shot attached I have selected the PCS0,1,2 however in the chip select configurations I have selected the SPI0_PCS0, 2 and 3. but not SPI0_PCS1.

My slaves devices are connected on SPI0_PCS0, SPI0_PC2, SPI0_PCS3 so I should be selecteding the Masterconfig with PCS0, PCS2, PCS3 right.

so by doing that and what you suggested doing an external init I am able to get a response from PCS2 and PCS3. but failed to get any response from PCS0 however, the PCS0 enable is going low. So is it that the MISO line is held low/ high impedance state by any other devices.

SPI without response.JPG

I am doing an external SPI Initialize using code below just before sending the first packet.

void InitializeSPI( void )

{

//    /* SIM_SCGC6: SPI0=1 */

//  SIM_SCGC6 |= SIM_SCGC6_SPI0_MASK;

//  /* Interrupt vector(s) priority setting */

////  /* NVICIP26: PRI26=0x70 */

////  NVICIP26 = NVIC_IP_PRI26(0x70);

////  /* NVICISER0: SETENA|=0x04000000 */

////  NVICISER0 |= NVIC_ISER_SETENA(0x04000000);

//    /* SIM_SCGC5: PORTD=1 */

//  SIM_SCGC5 |= SIM_SCGC5_PORTD_MASK;

//  /* PORTD_PCR3: ISF=0,MUX=2 */

//  PORTD_PCR3 = (uint32_t)((PORTD_PCR3 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR2: ISF=0,MUX=2 */

//  PORTD_PCR2 = (uint32_t)((PORTD_PCR2 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR1: ISF=0,MUX=2 */

//  PORTD_PCR1 = (uint32_t)((PORTD_PCR1 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR4: ISF=0,MUX=2 */

//  PORTD_PCR4 = (uint32_t)((PORTD_PCR4 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR5: ISF=0,MUX=2 */

//  PORTD_PCR5 = (uint32_t)((PORTD_PCR5 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR0: ISF=0,MUX=2 */

//  PORTD_PCR0 = (uint32_t)((PORTD_PCR0 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

//  /* PORTD_PCR6: ISF=0,MUX=2 */

//  PORTD_PCR6 = (uint32_t)((PORTD_PCR6 & (uint32_t)~(uint32_t)(

//                PORT_PCR_ISF_MASK |

//                PORT_PCR_MUX(0x05)

//               )) | (uint32_t)(

//                PORT_PCR_MUX(0x02)

//               ));

  /* SPI0_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=1,??=0,??=0,PCSIS=0x0F,DOZE=0,MDIS=0,DIS_TXF=0,DIS_RXF=0,CLR_TXF=0,CLR_RXF=0,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */

  SPI0_MCR = SPI_MCR_DCONF(0x00) |

             SPI_MCR_ROOE_MASK |

             SPI_MCR_PCSIS(0x0F) |

             SPI_MCR_SMPL_PT(0x00) |

             SPI_MCR_HALT_MASK;        /* Set Configuration register */

  /* SPI0_MCR: MSTR=1,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=1,??=0,??=0,PCSIS=0x0F,DOZE=0,MDIS=0,DIS_TXF=1,DIS_RXF=1,CLR_TXF=1,CLR_RXF=1,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */

  SPI0_MCR = SPI_MCR_MSTR_MASK |

             SPI_MCR_DCONF(0x00) |

             SPI_MCR_ROOE_MASK |

             SPI_MCR_PCSIS(0x0F) |

             SPI_MCR_DIS_TXF_MASK |

             SPI_MCR_DIS_RXF_MASK |

             SPI_MCR_CLR_TXF_MASK |

             SPI_MCR_CLR_RXF_MASK |

             SPI_MCR_SMPL_PT(0x00) |

             SPI_MCR_HALT_MASK;        /* Set Configuration register */

  /* SPI0_CTAR0: DBR=1,FMSZ=0x0F,CPOL=0,CPHA=0,LSBFE=0,PCSSCK=3,PASC=3,PDT=3,PBR=2,CSSCK=1,ASC=1,DT=1,BR=1 */

  SPI0_CTAR0 = SPI_CTAR_DBR_MASK |

               SPI_CTAR_FMSZ(0x07) |

               SPI_CTAR_PCSSCK(0x03) |

               SPI_CTAR_PASC(0x03) |

               SPI_CTAR_PDT(0x03) |

               SPI_CTAR_PBR(0x02) |

               SPI_CTAR_CSSCK(0x01) |

               SPI_CTAR_ASC(0x01) |

               SPI_CTAR_DT(0x01) |

               SPI_CTAR_BR(0x01);      /* Set Clock and Transfer Attributes register */

 

 

  /* SPI0_SR: TCF=1,TXRXS=0,??=0,EOQF=1,TFUF=1,??=0,TFFF=1,??=0,??=0,??=0,??=1,??=0,RFOF=1,??=0,RFDF=1,??=0,TXCTR=0,TXNXTPTR=0,RXCTR=0,POPNXTPTR=0 */

  SPI0_SR = SPI_SR_TCF_MASK |

            SPI_SR_EOQF_MASK |

            SPI_SR_TFUF_MASK |

            SPI_SR_TFFF_MASK |

            SPI_SR_RFOF_MASK |

            SPI_SR_RFDF_MASK |

            SPI_SR_TXCTR(0x00) |

            SPI_SR_TXNXTPTR(0x00) |

            SPI_SR_RXCTR(0x00) |

            SPI_SR_POPNXTPTR(0x00) |

            0x00200000U;               /* Clear flags */

  /* SPI0_RSER: TCF_RE=0,??=0,??=0,EOQF_RE=0,TFUF_RE=0,??=0,TFFF_RE=0,TFFF_DIRS=0,??=0,??=0,??=0,??=0,RFOF_RE=0,??=0,RFDF_RE=1,RFDF_DIRS=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  SPI0_RSER = SPI_RSER_RFDF_RE_MASK;   /* Set DMA Interrupt Request Select and Enable register */

  /* SPI0_MCR: HALT=0 */

SPI0_MCR &= (uint32_t)~(uint32_t)(SPI_MCR_HALT_MASK);

}

0 Kudos
Reply
4,666 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kewal,

I think you should first be sure whether the slave0 (connected to the PCS0) send reply.

From your screenshot we can see the M0SI work well , while the MISO have no data ,

so maybe the slave do not work well .

BR

Alice

0 Kudos
Reply
4,666 Views
Kewal
Contributor IV

Alice,

I have got it working now and the reason was the reset pin on the slave was tied to low,..  :smileysad:

Anwyays, since you earlier said

so  when you want select the other two slave SPI ,you can initialize them by hand refer to   the code under "comopnents_init".

or i think you can also use this function :

  DSPI_HAL_SetPcsPolarityMode(base, userConfig->whichPcs, userConfig->pcsPolarity);

so I was wondering how to actually switch between slaves.

        //Always consider camera instance

        DSPI_DRV_MasterDeinit(FSL_PCCPDSPICOM);

        DSPI_DRV_MasterInit(FSL_PCCPDSPICOM, &PCCPdspiCom_MasterState, &PCCPdspiCom_MasterConfig0);

        //Always consider camera instance

        DSPI_DRV_MasterDeinit(FSL_PCCPDSPICOM);

        DSPI_DRV_MasterInit(FSL_PCCPDSPICOM, &PCCPdspiCom_MasterState, &PCCPdspiCom_MasterConfig1);

0 Kudos
Reply