Re: UART and Thread

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: UART and Thread

1,926件の閲覧回数
ajaykr
Contributor I

Hi all,

Just now i tried the Uart-polling example with the same project,which is

working.I think the issues is with the interrupt.

 

On Mon, Dec 26, 2016 at 3:20 PM, Ajay K R <[email protected]> wrote:

 

Hi,

Thanks for reply.I'm using FRDM-64f board.First I checked my code alone

using the project uart non blocking,with interrupt and which is working

perfect.Then I moved the same code into the lwip tcp echo demo

project,which is now showing some issues.

 

      nRet = UART_DRV_Init(BOARD_DEBUG_UART3_INSTANCE, &uartState,

&uartConfig);

      pFunc = (uart_rx_callback_t *)uart_Callback;

      UART_DRV_InstallRxCallback(BOARD_DEBUG_UART3_INSTANCE

,(uart_rx_callback_t)pFunc ,&rxChar, 0, NULL);

      NVIC_SetPriority(I2C0_IRQn, 3U);

    while(true)

    {

     ReceiveCommandFromSerial();

     UART_DRV_ReceiveData(BOARD_DEBUG_UART3_INSTANCE , &rxChar , 8u);

    }

 

}

void uart_Callback()

{

__asm("nop");

}

If I use UART_DRV_SendData() function the whole board is getting hanging.

--

Regards

AJAY K R

 

 

 

 

--

Regards

AJAY K R

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,824件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello AJAY K R,

Thanks for your sharing.

So now one hand you can use the polling method,

on the other hand, if you must use interrupt, you need debug and analysis it

step by step , for example check whether the data have send , debug into

the function to check it hang which code ...

BR

Alice

0 件の賞賛
返信

1,824件の閲覧回数
ajaykr
Contributor I

Hi,

I conducted a step by step analysis,which shows a  UART_DRV_SendData() function is showing blocking the entire code.Suggest some solution to solve the issue with interrupt method.Polling method is not suitable for my application.

0 件の賞賛
返信

1,824件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

 You can share your project, then i debug on my side and check the problem.

BR

ALice

0 件の賞賛
返信