Preprocessor include macros don't work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Preprocessor include macros don't work

ソリューションへジャンプ
2,649件の閲覧回数
laszlomonda
Contributor IV

Hi there,

 

I'd like to use the preprocessor include macros feature of KDS to be able to build different firmware images on a per build profile basis for the various versions of our prototypes. Please see the following screenshot:

 

173367_173367.pngScreenshot from 2016-12-23 04-02-05.png

 

For some reason this doesn't work because:

  1. The exact same firmware image gets built as without the macro.
  2. In source code code editor the PROTOTYPE_VERSION_7 macro section gets grayed out instead of the else clause.

 

I'd be really grateful if someone could help me.

 

Thanks in advance!

 

- Laci

ラベル(1)
0 件の賞賛
返信
1 解決策
2,204件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Laci,

add your preprocessor symbols under the -D compiler (C, C++, assembler):

pastedImage_1.png

The other thing to know is: Eclipse uses the Indexer data base to gray out the sources. Depending on your project, I recommend you disable heuristics and rebuild the index, see Fixing the Eclipse Index | MCU on Eclipse 

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,204件の閲覧回数
laszlomonda
Contributor IV

Hi Erich, and Jennie,

Thank you so much for your help! Erich's instructions totally solved my problem.

Now I have only one question left: What is the preprocessor include macros feature of KDS supposed to do? It seems to me that it doesn't work.

Have a nice day,

Laci

0 件の賞賛
返信
2,204件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Laci,

In addition,  you can refer this article section2.1 with demo code:

How to support multiple targets in CodeWarrior(Classic, Eclipse)/KDS 

I referred Erich's article when writing this section
https://mcuoneclipse.com/2012/03/20/fixing-the-eclipse-index/

Hope this helps!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,204件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Laci,

add your preprocessor symbols under the -D compiler (C, C++, assembler):

pastedImage_1.png

The other thing to know is: Eclipse uses the Indexer data base to gray out the sources. Depending on your project, I recommend you disable heuristics and rebuild the index, see Fixing the Eclipse Index | MCU on Eclipse 

I hope this helps,

Erich

0 件の賞賛
返信