Pin Interrupt Processor Expert Init_GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin Interrupt Processor Expert Init_GPIO

Jump to solution
1,594 Views
martindusek
Contributor V

Hi,

I have difficulties getting pin interrupt on PTA12 of KL02 working. I configured Init_GPIO component, please see pictures of the configuration. I added interrupt service routine called OnChange to the main.c and at the beginning of this function I added breakpoint. However, when I connect PTA12 to GND (it has pull up) nothing happens - the breakpoint is not hit.

 

What else has to be done in order to have pin interrupt using Init_GPIO component working?

 

55973_55973.pngInit_GPIO.png55974_55974.pngInit_GPIO2.png55975_55975.pngInit_GPIO3.png

Labels (1)
0 Kudos
Reply
1 Solution
1,380 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Martin,

Please enable interrupt :

pastedImage_0.png

Hope it helps


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,381 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Martin,

Please enable interrupt :

pastedImage_0.png

Hope it helps


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------