Kinetis Design Studio IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Design Studio IDE

3,037 Views
doug_foss
Contributor I

I just downloaded Kinetis Design Studio IDE. I want to use the KL27Z parts and the FRDM-KL27Z board, but they are not listed in processor/board list. Is there a patch/update for this family of parts? If not, what is the closest other family to work with from a hardware/code standpoint?

Labels (1)
0 Kudos
Reply
3 Replies

2,731 Views
BlackNight
NXP Employee
NXP Employee

Additional devices are supported with the Kinetis SDK.

See "For full/additional device support"  in New Kinetis Design Studio V3.0.0 available

I hope this helps,

Erich

0 Kudos
Reply

2,731 Views
doug_foss
Contributor I

Erich,

Ok, thanks for that link. I am not able to do the Help>Install New Software successfully however. I get the messages in the attached screenshot. Is there a step that I need to perform before this, or maybe I need to reinstall the KDS?

Thanks,

Doug

0 Kudos
Reply

2,731 Views
BlackNight
NXP Employee
NXP Employee

I have seen such things with either slow or unreliable internet connections.

Maybe you can disable 'contact all update sites' (see Workaround for “Installing Software has encountered a problem” in Eclipse | MCU on Eclipse ) if this has a positive effect?

Erich

0 Kudos
Reply