Kinetis Design Studio 3.0.0 hangs on OSX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Design Studio 3.0.0 hangs on OSX

ソリューションへジャンプ
4,635件の閲覧回数
stefandzisiewsk
Contributor I

I've just started to transition to KDS from Codewarrior (my development cycles are intermittent). I have successfully installed and run KDS and created a new Kinetis project based around the FRDM-KL26Z. In Processor Expert view, when I uncheck "init" for any of the subsystems (for example ADC) the program hangs, giving me the spinning beachball of death.

 

The console output from KDS is:

 

29/09/2015 15:15:56.747 spindump[425]: Saved hang report for kinetis-design-studio version ??? (???) to /Library/Logs/DiagnosticReports/kinetis-design-studio_2015-09-29-151556_iMac2.hang

29/09/2015 15:15:57.285 SpotlightNetHelper[402]: [SLSUGGESTIONS] Location managed failed with error Error Domain=kCLErrorDomain Code=0 "The operation couldn’t be completed. (kCLErrorDomain error 0.)"

29/09/2015 15:15:58.446 kinetis-design-studio[1431]: WARNING: The Gestalt selector gestaltSystemVersion is returning 10.9.5 instead of 10.10.5. Use NSProcessInfo's operatingSystemVersion property to get correct system version number.

Call location:

29/09/2015 15:15:58.446 kinetis-design-studio[1431]: 0   CarbonCore                          0x00007fff8ae7a2b7 ___Gestalt_SystemVersion_block_invoke + 113

29/09/2015 15:15:58.446 kinetis-design-studio[1431]: 1   libdispatch.dylib                   0x00007fff861adc13 _dispatch_client_callout + 8

29/09/2015 15:15:58.446 kinetis-design-studio[1431]: 2   libdispatch.dylib                   0x00007fff861adb26 dispatch_once_f + 117

29/09/2015 15:15:58.446 kinetis-design-studio[1431]: 3   CarbonCore                          0x00007fff8ae03456 _Gestalt_SystemVersion + 987

29/09/2015 15:15:58.446 kinetis-design-studio[1431]: 4   CarbonCore                          0x00007fff8ae026e3 Gestalt + 144

29/09/2015 15:15:58.446 kinetis-design-studio[1431]: 5   kinetis-design-studio               0x00000001000019b4 main + 50

29/09/2015 15:15:58.446 kinetis-design-studio[1431]: 6   kinetis-design-studio               0x0000000100000fec start + 52

29/09/2015 15:16:04.297 com.apple.xpc.launchd[1]: (com.apple.imfoundation.IMRemoteURLConnectionAgent) The _DirtyJetsamMemoryLimit key is not available on this platform.

29/09/2015 15:16:27.258 WindowServer[237]: disable_update_timeout: UI updates were forcibly disabled by application "KDS" for over 1.00 seconds. Server has re-enabled them.

29/09/2015 15:16:27.323 WindowServer[237]: common_reenable_update: UI updates were finally reenabled by application "KDS" after 1.07 seconds (server forcibly re-enabled them after 1.00 seconds)

29/09/2015 15:17:09.709 com.apple.xpc.launchd[1]: (com.apple.quicklook[1440]) Endpoint has been activated through legacy launch(3) APIs. Please switch to XPC or bootstrap_check_in(): com.apple.quicklook

29/09/2015 15:17:35.000 kernel[0]: aio_queue_async_request(): too many in flight for proc: 16.

29/09/2015 15:17:38.000 kernel[0]: aio_queue_async_request(): too many in flight for proc: 16.

29/09/2015 15:18:01.000 kernel[0]: process kinetis-design-s[1431] thread 796521 caught burning CPU! It used more than 50% CPU (Actual recent usage: 73%) over 180 seconds. thread lifetime cpu usage 90.452741 seconds, (89.714209 user, 0.738532 system) ledger info: balance: 90004882413 credit: 90006969381 debit: 2086968 limit: 90000000000 (50%) period: 180000000000 time since last refill (ns): 123111712641

29/09/2015 15:18:01.556 com.apple.xpc.launchd[1]: (com.apple.ReportCrash[1443]) Endpoint has been activated through legacy launch(3) APIs. Please switch to XPC or bootstrap_check_in(): com.apple.ReportCrash

29/09/2015 15:18:01.557 ReportCrash[1443]: Invoking spindump for pid=1431 thread=796521 percent_cpu=73 duration=124 because of excessive cpu utilization

29/09/2015 15:18:02.260 spindump[425]: Saved cpu_resource.diag report for kinetis-design-studio version ??? (???) to /Library/Logs/DiagnosticReports/kinetis-design-studio_2015-09-29-151802_iMac2.cpu_resource.diag

 

I have attached the cpu_resource.diag report that this produced to this question too. This works fine in Windows, but I really would rather not have to run a VM just for this.

Original Attachment has been moved to: kinetis-design-studio_2015-09-29-151802_iMac2.cpu_resource.diag.zip

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
4,209件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Stefan,

I've logged the issue in our bug base under the number KDS-329

At this time I can not give you more info - release date.

Thanks for doing our product better.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
4,209件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Stefan,

I've a MAC with KDS + KSDK and PEx.

I0ve reproduced the problem on my side too.

As soon as I click on a Pin, the multicolor circle appears and ... loop forever.

Tool is not responding anymore.

Is it same issue ?


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,209件の閲覧回数
stefandzisiewsk
Contributor I

Hi Pascal

Yes, this is the same issue. Carlos, I have attached an image of where the error occurs with the checkbox that causes the hang circled in red.

Screen Shot 2015-09-29 at 15.17.09 copy.png

Hope this helps

S

0 件の賞賛
返信
4,210件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Stefan,

I've logged the issue in our bug base under the number KDS-329

At this time I can not give you more info - release date.

Thanks for doing our product better.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,209件の閲覧回数
stefandzisiewsk
Contributor I

Thanks for this Pascal - let me know if there's any further info I can provide.

All the best

Stefan

0 件の賞賛
返信
4,209件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Stefan,

I've the same problem on my side.

I'm trying to install all patches but got errors to install PEx and KSDK patches.

I will check if there is another way to get them just to be sure if the problem is not already solved.

Keep you informed.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,209件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Stefan,

Could you tell us which OSX version are you using? Please notice that the host operating systems supported by KDS are:

• Windows® 7/8 (32-bit binaries running on 32 and 64-bit OS).

• Linux® (Ubuntu 14.04 (deb), RedHat/Centos 7 (rpm)) (64 bit binaries).

• Mac OS X ("Yosemite") with Segger support.

Best Regards!

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信
4,209件の閲覧回数
stefandzisiewsk
Contributor I

Hi Carlos

OS X version is Yosemite 10.10.5. All other aspects of KDS work, it's just I can't use Processor Expert because of this - but I am actually getting good results without, so it's not a huge issue for me, but might be for others.

S

0 件の賞賛
返信
4,209件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Stefan,

Thanks for your response.

Could you post an screenshot of the init setting you change on the component before KDS hangs?

Best Regards!

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信