KDS 3.0.0 AsynchroSerial Connect Pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KDS 3.0.0 AsynchroSerial Connect Pin

跳至解决方案
3,046 次查看
ETCTim
Contributor I

I am attempting to share the TX Pin of a uart of a 120mhz K70.

I have an AsynchroSerial component setup and have the pin shared.

When I generate PE code with the ConnectPin method set to be generated, I get a generator failure error.

 

Description Resource Path Location Type

Generator: FAILURE: at line 228: Error in including "Drivers\Common\SynchroMasterConnectPin.inc" from directory C:\Freescale\KDS_3.0.0\eclipse\ProcessorExpert\Repositories\Kinetis_Repository (file: Drivers\Kinetis\AsynchroSerial.drv) Series3MQXLiteKDS  DMXSerial Processor Expert Problem

 

This worked fine in CW 10.6

It seems weird that the ASychro component is looking for the SynchroMasterConnectPin file

 

Any ideas on how to fix this. It also seems to happen on a K10 project.

 

Tim

标签 (1)
0 项奖励
回复
1 解答
2,781 次查看
marek_neuzil
NXP Employee
NXP Employee

Hello Tim,

The hot fix is prepared and verified in the KDS 3.0.0 - PEx for Kinetis 3.0.1.

I have attached the hot fix to this response, see the file.

Best Regards,

Marek Neuzil

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,781 次查看
marek_neuzil
NXP Employee
NXP Employee

Hello,

Thank you for reporting of this defect. It is a bug in the AsynchroSerial.drv driver (incorrect include file is used). I have reported this issue to the responsible Processor Expert development team. There should be a hot fix provided soon.

Best Regards,

Marek Neuzil

0 项奖励
回复
2,781 次查看
ETCTim
Contributor I

Thanks Marek,

Any idea on the when a fix will be available?

Thanks,

Tim

0 项奖励
回复
2,782 次查看
marek_neuzil
NXP Employee
NXP Employee

Hello Tim,

The hot fix is prepared and verified in the KDS 3.0.0 - PEx for Kinetis 3.0.1.

I have attached the hot fix to this response, see the file.

Best Regards,

Marek Neuzil

0 项奖励
回复
2,781 次查看
ETCTim
Contributor I

Thank you. It seems to have fixed it.

0 项奖励
回复
2,781 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Tim,

thank you for posting the problem.

can you please send us the KDS demo project and error screenshot? I will check the problem directly on my side. thanks!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复