KDS 3.0.0 AsynchroSerial Connect Pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS 3.0.0 AsynchroSerial Connect Pin

Jump to solution
3,021 Views
ETCTim
Contributor I

I am attempting to share the TX Pin of a uart of a 120mhz K70.

I have an AsynchroSerial component setup and have the pin shared.

When I generate PE code with the ConnectPin method set to be generated, I get a generator failure error.

 

Description Resource Path Location Type

Generator: FAILURE: at line 228: Error in including "Drivers\Common\SynchroMasterConnectPin.inc" from directory C:\Freescale\KDS_3.0.0\eclipse\ProcessorExpert\Repositories\Kinetis_Repository (file: Drivers\Kinetis\AsynchroSerial.drv) Series3MQXLiteKDS  DMXSerial Processor Expert Problem

 

This worked fine in CW 10.6

It seems weird that the ASychro component is looking for the SynchroMasterConnectPin file

 

Any ideas on how to fix this. It also seems to happen on a K10 project.

 

Tim

Labels (1)
0 Kudos
Reply
1 Solution
2,756 Views
marek_neuzil
NXP Employee
NXP Employee

Hello Tim,

The hot fix is prepared and verified in the KDS 3.0.0 - PEx for Kinetis 3.0.1.

I have attached the hot fix to this response, see the file.

Best Regards,

Marek Neuzil

View solution in original post

0 Kudos
Reply
5 Replies
2,756 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

Thank you for reporting of this defect. It is a bug in the AsynchroSerial.drv driver (incorrect include file is used). I have reported this issue to the responsible Processor Expert development team. There should be a hot fix provided soon.

Best Regards,

Marek Neuzil

0 Kudos
Reply
2,756 Views
ETCTim
Contributor I

Thanks Marek,

Any idea on the when a fix will be available?

Thanks,

Tim

0 Kudos
Reply
2,757 Views
marek_neuzil
NXP Employee
NXP Employee

Hello Tim,

The hot fix is prepared and verified in the KDS 3.0.0 - PEx for Kinetis 3.0.1.

I have attached the hot fix to this response, see the file.

Best Regards,

Marek Neuzil

0 Kudos
Reply
2,756 Views
ETCTim
Contributor I

Thank you. It seems to have fixed it.

0 Kudos
Reply
2,756 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Tim,

thank you for posting the problem.

can you please send us the KDS demo project and error screenshot? I will check the problem directly on my side. thanks!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply