KDS 3.0.0 AsynchroSerial Connect Pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS 3.0.0 AsynchroSerial Connect Pin

ソリューションへジャンプ
2,973件の閲覧回数
ETCTim
Contributor I

I am attempting to share the TX Pin of a uart of a 120mhz K70.

I have an AsynchroSerial component setup and have the pin shared.

When I generate PE code with the ConnectPin method set to be generated, I get a generator failure error.

 

Description Resource Path Location Type

Generator: FAILURE: at line 228: Error in including "Drivers\Common\SynchroMasterConnectPin.inc" from directory C:\Freescale\KDS_3.0.0\eclipse\ProcessorExpert\Repositories\Kinetis_Repository (file: Drivers\Kinetis\AsynchroSerial.drv) Series3MQXLiteKDS  DMXSerial Processor Expert Problem

 

This worked fine in CW 10.6

It seems weird that the ASychro component is looking for the SynchroMasterConnectPin file

 

Any ideas on how to fix this. It also seems to happen on a K10 project.

 

Tim

ラベル(1)
0 件の賞賛
返信
1 解決策
2,708件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello Tim,

The hot fix is prepared and verified in the KDS 3.0.0 - PEx for Kinetis 3.0.1.

I have attached the hot fix to this response, see the file.

Best Regards,

Marek Neuzil

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,708件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

Thank you for reporting of this defect. It is a bug in the AsynchroSerial.drv driver (incorrect include file is used). I have reported this issue to the responsible Processor Expert development team. There should be a hot fix provided soon.

Best Regards,

Marek Neuzil

0 件の賞賛
返信
2,708件の閲覧回数
ETCTim
Contributor I

Thanks Marek,

Any idea on the when a fix will be available?

Thanks,

Tim

0 件の賞賛
返信
2,709件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello Tim,

The hot fix is prepared and verified in the KDS 3.0.0 - PEx for Kinetis 3.0.1.

I have attached the hot fix to this response, see the file.

Best Regards,

Marek Neuzil

0 件の賞賛
返信
2,708件の閲覧回数
ETCTim
Contributor I

Thank you. It seems to have fixed it.

0 件の賞賛
返信
2,708件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Tim,

thank you for posting the problem.

can you please send us the KDS demo project and error screenshot? I will check the problem directly on my side. thanks!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信