J-Link GDB Server failed dialog

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

J-Link GDB Server failed dialog

17,499件の閲覧回数
laszlomonda
Contributor V

Hi guys,

 

From time to time, the following error dialog appears when trying to download the firmware to an FRDM board:

 

143740_143740.pngproblem-occured-dialog.png

 

This is a major productivity problem for me, because the only way to reliably recover from this error is to detach the board, exit and re-launch KDS, attach the board, and re-download the firmware. Sometimes I'm able to download the firmware about a dozen times in a row without bumping into this error, other times it occurs almost every time.

 

The content of the JLinkGDBServerCL console:

 

SEGGER J-Link GDB Server V4.98b Command Line Version

 

JLinkARM.dll V4.98b (DLL compiled Apr 10 2015 20:27:35)

 

-----GDB Server start settings-----

GDBInit file:                  none

GDB Server Listening port:     2331

SWO raw output listening port: 2332

Terminal I/O port:             2333

Accept remote connection:      localhost only

Generate logfile:              off

Verify download:               on

Init regs on start:            on

Silent mode:                   off

Single run mode:               on

Target connection timeout:     0 ms

------J-Link related settings------

J-Link Host interface:         USB

J-Link script:                 none

J-Link settings file:          none

------Target related settings------

Target device:                 MK22FN512xxx12

Target interface:              SWD

Target interface speed:        30kHz

Target endian:                 little

 

Connecting to J-Link...

J-Link is connected.

Firmware: J-Link OpenSDA 2 compiled Oct 13 2015 12:10:56

Hardware: V1.00

S/N: 621000000

Checking target voltage...

Target voltage: 3.30 V

ERROR: Failed to bind address (Err = 98)

ERROR: Failed to open listener port 2331

Restoring target state and closing J-Link connection...

Shutting down...

 

Thank you very much in advance!

- Laci

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

11,304件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

there is customer having similar problem as yours. he solved the problem with below thread:

arm-none-eabi-edb.exe in KDS 3.0.0 failing after J-link firmware update

can it also work for you?
Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

11,304件の閲覧回数
bosleymusic_com
Contributor IV

KDS 3.1.0 is suddenly failing with Segger J-Link plus - I had no problem for weeks, and all of a sudden I'm getting this :

pastedImage_0.png

Have tried shut down, restart, unplugging, etc... J-Link Commander works freely on its own, but still nothing with KDS. I haven't installed anything new, I haven't changed any settings, windows hasn't updated, so I don't understand how this is magically happening all of a sudden. Any suggestions? 

Console Details :

GNU gdb (GNU Tools for ARM Embedded Processors) 7.6.0.20140731-cvs

Copyright (C) 2013 Free Software Foundation, Inc.

License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>

This is free software: you are free to change and redistribute it.

There is NO WARRANTY, to the extent permitted by law.  Type "show copying"

and "show warranty" for details.

This GDB was configured as "--host=i686-w64-mingw32 --target=arm-none-eabi".

For bug reporting instructions, please see:

<http://www.gnu.org/software/gdb/bugs/>.

Warning: the current language does not match this frame.

/home/build/work/GCC-4-8-build/src/gdb/gdb/linespec.c:2445: internal-error: decode_line_full: Assertion `state->canonical_names[i].suffix != NULL' failed.

A problem internal to GDB has been detected,

further debugging may prove unreliable.

Quit this debugging session? (y or n) [answered Y; input not from terminal]

/home/build/work/GCC-4-8-build/src/gdb/gdb/linespec.c:2445: internal-error: decode_line_full: Assertion `state->canonical_names[i].suffix != NULL' failed.

A problem internal to GDB has been detected,

further debugging may prove unreliable.

Create a core file of GDB? (y or n) [answered Y; input not from terminal]

This application has requested the Runtime to terminate it in an unusual way.

Please contact the application's support team for more information.

0 件の賞賛
返信

11,304件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I just wrote an article about FRDM-K22F debug interface.

Summary of FRDM-K22F debug interface

Hope this can help you.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

11,304件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

what KDS version do you work with?

do you use NXP FRDM board or external J-link tool?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

11,304件の閲覧回数
laszlomonda
Contributor V

Hi Jennie,

I use KDS 3.1.0 with the internal OpenSDA programming port of the FRDM boards, without an external programmer.

Thank you!

- Laci

0 件の賞賛
返信

11,302件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Laci,

from my understanding, you use FRDM-K22 board, I suggest you update your board firmware with JLink_OpenSDA_V2_1_2015-10-13.bin (see attached) then test it again.

if still can not connect, I suggest you download and install the latest J-Link software package

https://www.segger.com/jlink-software.html

Segger J-Link OpenSDA Firmware update procedure:

  1. Disconnect all power, external circuits and USB cables.
  2. Press and hold the button marked RESET (circled in picture)
  3. Connect a USB cable with debug interface as shown in above picture
  4. The drive should mount named BOOTLOADER in windows explore
  5. The reset button can now be released
  6. Drag and drop the file JLink_OpenSDA_V2_1_2015-10-13.bin onto the USB drive named BOOTLOADER
  7. Repower on board normally
  8. Jlink CDC UART Port will show up in windows device manager.
  9. Then user can download and debug code via KDS3.0 debugger Segger J-Link OpenSDA interface.

if jlink interface can not work for you anyway, I suggest you try P&E OpenSDA. the bootloader image is also attached.

can it help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

11,302件の閲覧回数
laszlomonda
Contributor V

Thank you very much for your help, Jennie!

Actually, I was already using the latest J-Link OpenSDA firmware. I've given P&E a try this time but it seems that it's not better. It takes about 10 seconds to download the firmware to the board, and I get "Error in services launch sequence" error message very often.

Cheers!

0 件の賞賛
返信