Importing FRDM-KE02Z Example Project into KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Importing FRDM-KE02Z Example Project into KDS

1,933 Views
aboss
Contributor I

I have a FRDM-KL02Z evaluation board, along with the downloaded example projects. When I import an example project into KDS, I first must convert it from a Code Warrior project to a KDS project. Upon compiling, I am getting 3 warnings:

Capture.PNG

These same errors occur regardless of which project I import. Any help would be much appreciated.

-Andrew

Tags (1)
0 Kudos
Reply
1 Reply

1,748 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andrew,

There is a tutorail  about porting project from CW to KDS, you can have a look :

Importing MCU V10.6 projects (sample, using PE and MQX) under KDS 

If can't work ,I recommendy you directly create a new project on KDS, then copy&paste the application code

into it .

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply