FreeRTOS or MQX? - Problems while importing RTOS using Processor Expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FreeRTOS or MQX? - Problems while importing RTOS using Processor Expert

2,104 次查看
vishalgirisagar
Contributor II

Hello,

 

 

1.  I want to use RTOS for my application. I am using Kinetis series K22FN512 MCU. Which RTOS is better? 

 

2. Is Processor Expert free of cost. ? If yes, I got following error today -

Jun 9, 2015 4:38:49 PM Starting Processor Expert service

System directory = C:\Freescale\KDS_3.0.0\eclipse\ProcessorExpert

Internal cache directory = C:\ProgramData\Processor Expert\PECache\6e5874fa

Processor Expert license file = not used (no license file)

 

3. Also I am using Kinetis Design Studio IDE for compiling. I am facing some weird problems. Not able to see "Kinetis SDK", "Free RTOS" and "MQX" in component library. I am following the tutorial in below link. Please help me.

 

Tutorial: FreeRTOS with the Kinetis SDK and Processor Expert | MCU on Eclipse

 

 

36317_36317.pngpastedImage_2.png

 

36318_36318.pngpastedImage_3.png

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,722 次查看
vfilip
NXP Employee
NXP Employee

Hi,

please select your RTOS within fsl_os_abstraction component (OSA). Details below:

pastedImage_0.png

RTOS preference is up to you, I would select FreeRTOS.

There exists now two FreeRTOS components. One is delivered by default with PEx for KSDK 1.2.0 second is developed within MCU online page. Components from this page must be installed extra.

best regards

Vojtech Filip

0 项奖励
回复

1,722 次查看
vishalgirisagar
Contributor II

Hi Vojtech,

  Thanks for your reply. I understand how to select the RTOS now. Can you please tell me why would you  choose FreeRTOS? Any specific reason? I mean the pros can influence me to choose it. But I want to know reason.

0 项奖励
回复