Display analog data in Kinetis Design Studio?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Display analog data in Kinetis Design Studio?

ソリューションへジャンプ
1,997件の閲覧回数
christopherira
Contributor III

Hi,

 

I want to display the data being converted on my ADC pin on Kinetis Design Studio. I know there's expressions and variables, but it doesn't seem to work while I'm running my debug, only while it's paused, plus I can't interpret the data. plus it only gives me one value not a whole stream of values.

141291_141291.pngpastedImage_0.png

 

Thanks for your time,

-Chris

ラベル(1)
0 件の賞賛
返信
1 解決策
1,796件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Chris,

In KDS, it can not refresh variable while running , while there is a method close to

this function, you can refer to .

Re: KDS refresh variable while running KEA128

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,797件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Chris,

In KDS, it can not refresh variable while running , while there is a method close to

this function, you can refer to .

Re: KDS refresh variable while running KEA128

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------