Data Logging in KEA-128?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Data Logging in KEA-128?

1,160 Views
vigneshbalaji
Senior Contributor I

Hi,

    Is it possible to log CAN data over KEA-128. Giving the Fact that KEA-128 has only 128 K OF Flash Memory???

Is there any work around for this?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

936 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Vignesh

128 K flash is enough to run a CAN application. The Data Filed in each frame is up to 64bit.  The MSCAN module on KEA128 supports 5 receive buffers and 3 transmit buffers.

How many records would you preserved on flash?

There has an MSCAN driver for KEA128, it can be downloaded  from :

http://cache.nxp.com/files/microcontrollers/software/device_drivers/MSCAN_KEA_DEVD.zip


Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply