Data Logging in KEA-128?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Data Logging in KEA-128?

1,157件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

    Is it possible to log CAN data over KEA-128. Giving the Fact that KEA-128 has only 128 K OF Flash Memory???

Is there any work around for this?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

933件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Vignesh

128 K flash is enough to run a CAN application. The Data Filed in each frame is up to 64bit.  The MSCAN module on KEA128 supports 5 receive buffers and 3 transmit buffers.

How many records would you preserved on flash?

There has an MSCAN driver for KEA128, it can be downloaded  from :

http://cache.nxp.com/files/microcontrollers/software/device_drivers/MSCAN_KEA_DEVD.zip


Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信