Converting Code Warrior10.6 project in KDS not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Converting Code Warrior10.6 project in KDS not working

1,285件の閲覧回数
pallenna
Contributor II

Hi to all,

i am new to KDS IDE. i tried to importing a existing project from the Codewarrior 10.6 to KDS,and i followed the procedure of Importing MCU V10.6 projects (sample, using PE and MQX) under KDS, but it is not working. and i getting error as follows

make: *** [Test_TWR_K60DM100.elf] Error 1.

and i am sending the attachment please check it once,in this file if i did any mistakes please mention.

 

Thanks and Regards,

padmaja


ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,064件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Pallenna,

Please take a look to the answer on your other post:

Converting Code Warrior10.6 project in KDS not working

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信