Codewarrior Peoject To KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior Peoject To KDS

1,782 Views
salah
Contributor III

Dear All,

I am using Codewarrior 10.6 for TWR-KW24D512 boards. I would like to try KDS instead codewarrior. How can I transfer code warrior project to KDS and configure the board? Please help

 

Thanks!

Salah

Labels (1)
0 Kudos
Reply
2 Replies

1,644 Views
TICS_Fiona
NXP Employee
NXP Employee

To Import the project I did in KDS: File-> Import-> Existing Projects Into Workspace and then I selected the project I created in CodeWarrior. Once the project is imported I did right click on it and I selected "convert CodeWarrior project file."

For details you may refer to the documents below:

http://cache.freescale.com/files/microcontrollers/doc/user_guide/KDSPGQS.pdf

https://community.freescale.com/docs/DOC-102594

Hope it helps!

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,644 Views
salah
Contributor III

Hi Fiona,

I just replied the SR with More information. Please take a look. I am still getting this error:

Description    Resource    Path    Location    Type

make: *** No rule to make target `MyWirelessApp Demo End Device - Security Enabled.elf', needed by `main-build'.  Stop.    MyWirelessApp Demo End Device - Security Enabled             C/C++ Problem

I am trying a demo which was generated using Beekit to CW.

Thanks,
Salah

0 Kudos
Reply