Changing the Power Modes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing the Power Modes

ソリューションへジャンプ
1,454件の閲覧回数
syed_idris
Contributor III

Hi,
We are working on KL03 with KDS3.1.0 + PE, 
As I can see in datasheet there are power modes available as Normal Run, Normal Wait, Normal Stop, VLPR, VLPW etc..
Please guide me how can I change the power modes of the KL03 in programming using KDS IDE,

Or is there document/ tutorial for changing the power modes using KDS programming?

 

Regards,
Idris

ラベル(1)
1 解決策
1,345件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Idris,

The attachment is a demo on CodeWarrior  +PE , it is the same with KDS.

You can  open it on CW, then create one new project on KDS, refer to the demo to develop.


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,346件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Idris,

The attachment is a demo on CodeWarrior  +PE , it is the same with KDS.

You can  open it on CW, then create one new project on KDS, refer to the demo to develop.


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------