Bug: KDS fails to start debug with "Error in final launch sequence"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug: KDS fails to start debug with "Error in final launch sequence"

998件の閲覧回数
davenadler
Senior Contributor I

K64F Freedom board, latest KDS (all updates as of last week).
Debug was working OK and suddenly I get the following error when trying to launch debugger:
170487_170487.PNGKDS OpenOCD fails to start debug.PNG

If I power-cycle the board I can drag-and-drop a "hello world blinky light" application into the mbed drive and it works, so the board seems to be OK. There are no zombie debug processes (the problem happens every time on clean start of KDS and board).

 

Anybody have any idea what's going on?

Thanks,
Best Regards, Dave

 

PS: Alice, please do not suggest I re-install Windows or other silliness.

PPS: The following users have reported related problems with no problem resolution:

https://community.nxp.com/message/832787

https://community.nxp.com/message/832828

https://community.nxp.com/message/665363

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

863件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Dave,

is this the same issue as https://community.nxp.com/thread/439738 ?

if yes please refer above thread of my response.

Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信