BUG: Pin Expert losing critical data!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BUG: Pin Expert losing critical data!

1,260 次查看
davenadler
Senior Contributor II

Kinetis Expert, PC version, *** About NXP Configuration Tools: Installed tools: Pins (2.0) Clocks (1.0)

Yesterday I used Pin Expert, exported pin_mux.h and pin_mux.c, and saved MEX file.
Project built and ran perfectly.

 

Today I use the same MEX file, but many pin names are missing.
For example the symbol BOARD_INITMFW2_POWER_RAIL_ON_OFF_GPIO.
If I export the c/h files, my project no longer builds!

 

If I start Pin Expert and import yesterday's working pin_mux.h and pin_mux.c files,
it does not import many definitions including BOARD_INITMFW2_POWER_RAIL_ON_OFF_GPIO.

 

In the attached ZIP are the generated files from yesterday (which are OK), and the MEX file (which if loaded seems to have lost lots of definitions).

 

HELP!!!
Thanks,
Best Regards, Dave

Original Attachment has been moved to: uC_setup_20170126_working.zip

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,043 次查看
MarekTrmac
NXP Employee
NXP Employee

Hi Dave,

community for Kinetis Expert tools and MCUxpresso Configuration tools is here: https://community.nxp.com/community/mcuxpresso/mcuxpresso-config

Regards

Marek

0 项奖励
回复