I'm having include problems when compiling the IOT Mavlink Module.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I'm having include problems when compiling the IOT Mavlink Module.

ソリューションへジャンプ
2,922件の閲覧回数
nxf58541
NXP Employee
NXP Employee

Has anybody experienced the following error while buildiung the MAVLink IoT module build? Have fixed all the macro errors: https://imgur.com/a/uLN5wyL. Unresolved inclusion of #include "./mavlink_msg_change_operator_control.h"
No such file or directory found.

0 件の賞賛
返信
1 解決策
2,889件の閲覧回数
nxf58541
NXP Employee
NXP Employee

The example code is working with PX4 1.10 in its current state.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,890件の閲覧回数
nxf58541
NXP Employee
NXP Employee

The example code is working with PX4 1.10 in its current state.

0 件の賞賛
返信