I'm having include problems when compiling the IOT Mavlink Module.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I'm having include problems when compiling the IOT Mavlink Module.

Jump to solution
2,951 Views
nxf58541
NXP Employee
NXP Employee

Has anybody experienced the following error while buildiung the MAVLink IoT module build? Have fixed all the macro errors: https://imgur.com/a/uLN5wyL. Unresolved inclusion of #include "./mavlink_msg_change_operator_control.h"
No such file or directory found.

0 Kudos
Reply
1 Solution
2,918 Views
nxf58541
NXP Employee
NXP Employee

The example code is working with PX4 1.10 in its current state.

View solution in original post

0 Kudos
Reply
1 Reply
2,919 Views
nxf58541
NXP Employee
NXP Employee

The example code is working with PX4 1.10 in its current state.

0 Kudos
Reply