I'm having include problems when compiling the IOT Mavlink Module.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I'm having include problems when compiling the IOT Mavlink Module.

跳至解决方案
2,172 次查看
nxf58541
NXP Employee
NXP Employee

Has anybody experienced the following error while buildiung the MAVLink IoT module build? Have fixed all the macro errors: https://imgur.com/a/uLN5wyL. Unresolved inclusion of #include "./mavlink_msg_change_operator_control.h"
No such file or directory found.

0 项奖励
回复
1 解答
2,139 次查看
nxf58541
NXP Employee
NXP Employee

The example code is working with PX4 1.10 in its current state.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,140 次查看
nxf58541
NXP Employee
NXP Employee

The example code is working with PX4 1.10 in its current state.

0 项奖励
回复